您好:
我想找个pin-to-pin的电源芯片 5V输入,固定1.8V输出,输出电流200mA左右,管脚定义如下:1:EN 2:GND 3:SW 4: IN 5:OUT
能否推荐
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,根据您给出的要求以下两颗能满足您的要求。
TPS62202 Input voltage range 2.5V to 6.0V,Maximum output current 300mA,Vout=1.8V, Package: 5Pin SOT-23
http://www.ti.com.cn/cn/lit/ds/symlink/tps62202.pdf
TPS62222 Input voltage range 2.5V to 6.0V,Maximum output current 400mA,Vout=1.8V, Package: 5Pin SOT-23
http://www.ti.com.cn/cn/lit/ds/symlink/tps62222.pdf
能否告知原料的料号及封装,以及更多应用相关指标信息,以便为您进一步推荐。谢谢!