Other Parts Discussed in Thread: UC2843, LM2587, LM2588, TPS40210, TPS28225, UCC2897A, LMV431A, LM258
您好,麻烦请推荐一款电源芯片,输入18-36V,输出24V,输入与输出带隔离功能,类似于DCDC隔离电源模块
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
如果电流不大,或许你可以参考一下这个设计
您好,
根据您的需求,在TI的官网上powerlab工具中有一些相应的参考设计,用到诸如TPS40210的flyback, 满载电流在3A,效率91%,还有有源箝位电路,用到TPS28225+UCC2897A,以及一些其他的参考设计。原理图,PCB等都可以在上面下到。
您好,
您的这个想法很好,从您的设计也可以看出您需要18~30V的输入,24V@1.2A的输出,输出需要隔离。
有两点要提醒的是,LM2588是峰值电流控制,自带输入电压前馈,并不需要再接一个反馈,建议将光耦的反馈接到FB。
另外一点则是光耦由于在传输过程中存在较大的误差,所以需要在光耦的前端添加431的反馈网络。这样,反馈网络能及时调整光耦的误差。TI也有您需要的LMV431A。
希望这些能帮助到您。谢谢。
谢谢您的回复,我还想问下T1的体积大概是多大?因为我的板子对高度有要求。