Other Parts Discussed in Thread: BQ76PL536, MSP430F5529
是否有电动汽车电池管理的相关解决方案资料?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好,购买的事宜请在EVM板主页的“立即订购”栏 点击从“TI购买”可以进入到TI E-store进行购买的操作。
使用430比较方便的一点是TI提供了它与BQ76PL536通讯的参考代码(参考http://www.ti.com/lit/zip/slaa478.),同时能够通过RS232/RS485/
USB-CDC Class这些接口与外围控制器直接通讯。
如果项目要求一定要通过Can总线通讯,同时希望集成度能够更加高一些,那么可以考虑将MSP430芯片换成一个C2000的芯片,相比430单片机,由于C2000内部集成了Can总线的控制器模块,所以只要外部加一个Can总线收发器就可以了,同时它也可以直接与BQ76PL536通过SPI口通讯,但C2000的价格比430单片机会贵一些。