This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

需要设计一个DC 22V-28V输入,DC72V 100mA输出 纹波要求0.1mV,输出稳定性0.01%@8小时的电源

Other Parts Discussed in Thread: LM5001, TL783

          需要设计一个DC 22V-28V输入,DC72V 100mA输出 纹波要求0.1mV,输出电压可调,输出稳定性0.01%@8小时的电源,TI有什么方案可以推荐。

可以电话或者邮件联络我。

          用于探测器供电,输出电源电压68V-75V可调,要求电源输出电压稳定,方案实现成本作为最后考虑选项,接受分立器件方案及多级方案。