This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS40210芯片方案能否输出-100VDC?

Other Parts Discussed in Thread: TPS40210, LM2588

    TI专家,您好

      TI的TPS40210这款芯片方案中有20~30V转100V/280mA的方案:http://www.ti.com.cn/tool/cn/pmp8913   我想请问一下是否可以修改一下方案电路,使得输出-100V/280mA(输出负100V)。 本人对设计电源没有经验,在网上看到一些开关电源的设计资料(如下图)。把电感的位置换一下就可以得到负压???如果真是这样,20~30V转100V/280mA的方案中只要改变一下电感L1的位置就可以了吗?

    公司现在需要设计一块24VCDC或12VDC转+/-100VDC的高压板,输出电流200mA左右就可以了。如果TI公司有其他方案,请麻烦指点一下。谢谢