This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ34Z110求助4

  • TI技术支持:

我收到了2014.2.11号回复的帖子,非常感谢!

我买到了BQ34Z110用于铅酸电池的片芯,根据BQ34Z110用户手册进行了针对型号为超威6-DZM-20,容量为20AH的铅酸蓄电池进行电量计的开发.CHEM ID 选为0800,OCV TABLE表采用默认值.没有通过EV2300下载相应的固件到BQ34Z110.经过反复试验,QMAX已经更新,阻抗表也已生成,UPDATA STATUS已变为06.但是,在测试超威6-DZM-20蓄电池放电精度时发现,SOC的值会常时间停留在某一个值上.例如停在SOC=10或者SOC=6的位置.直到蓄电池端电压降到终止电压10800时才能使SOC=0,RM=0.为此希望请教以下问题:

1)   出现上述的原因是什么?如何才能解决呢?

2)    您的回帖中说选择一个化学性质相似的CHEM ID.目前对于铅酸蓄电池0800系列的CHEM ID(已有8000--8007).但还没有这样相近的CHEM ID .我应该如何继续进行开发!

3)   我在超威蓄电池上作的开发的"黄金文件"是否可用于其它厂家同类电池上,例如用于天能6-DZM-20.

谢谢!

  • 1)有可能是因为内部计算通过电量的寄存器溢出,你可以试一下在SOC=10的时候静置2小时,然后放电看SOC是否能正常下降,如果可以的话那么应该是这个问题,解决方式只能通过比例缩放的方式,即在校准电流时输入的电流数值以及填写设计容量等都缩小2倍填写。

    2)这个CHEM-ID的是否相近你是通过MATHCAD工具计算得到的?

    3)需要重新做golden file