This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq34z110问题7

Other Parts Discussed in Thread: BQ34Z110, EV2400

TI技术支持:

在开发BQ34Z110中有几个问题希望能得到您的解答:

1)   SENC文件,DFI文件,ROM文件分别是什么文件,如何分别获得呢?

2)   如果BQ34Z110学习成功,UPDATE STATUS 变为06之后,为什么必须人工将RA  MAX  DELTA参数修改到RA_TABLT格点4的值的15%?

改变黄金DFI文件时怎么又要将RA  MAX  DELTA参数修改到RA_TABLE格点4的值的20? 这到底是个什么概念?

3)   如果BQ34Z110学习成功后,在正常运行中需要启动0021命令吗?为什么必须将SENC文件中的UPDATE  STATUS 从06改为02?

谢谢!

  • 1)senc dfi文件通过我们上位机软件EVSW配合EV2300/EV2400可以导出

    2)这个只是限制一下Ra每次更新的范围而已,能否给出这段话的原文出处?

    3)之所以改成02的目的是因为防止在组装过程中(比如焊接等工序)一些异常的电压电流造成电量计计算误差或者life data数据被记录,所以等到组装PACK后就可以发送21命令使能IT算法,在后续使用中无需再次发送

    另外建议把相关问题都发在同一个帖子中,谢谢!