用TI的lm2841或者2842的芯片,datasheet上面给的电路图比如输入12V输出5V的话,那么输入电压降低时,输出电压会成比例的降低还是一直保持着5V的输出(保持电路图不变的话)吗?希望可以得到大家的帮忙,谢谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
根据Vout=0.765V(1+(R1/R2)可得,输出电压的大小取决于反馈电阻R1和R2的比值,和输入无关。
william miqi 说:那也就是说LM2841的datasheet上的应用电路不能用来成比例的降压,只是为了做成一个稳压电源输出?
只要输入不欠压,输入变化时,输出电压还是稳定的。