This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

bq25070充电电流

Other Parts Discussed in Thread: BQ25070, TPS62143

用bq25070给单节LiFePO4电池充电,电流设定在935mA. 串联0.01ohm的电阻可以量测实际充电电流。

给空电池充电,开始几分钟充电电流是935mA, 但是几分钟以后电流会降到794mA,不知道这个电流为什么不能稳定935mA.

  • 你好,你的输入电压是多少?是否有很长的输入导线,建议你将输入电压增加一些验证是否能保持在935mA。谢谢!

  • 输入电压是5V,用TPS62143给bq25070供电。在同一个PCB上。

    把bq25070的充电电流设定在654mA,  电流也会往下掉。

    有没有可能是温度太高了,bq25070会自动调节充电电流。bq25070的温度很高,估计超过90度。

    但是bq25070上没有接NTC. NTC接在电量计bq27500上, 用470K和100K的电阻接在bq25070的TS上。

  • 应该是die温度过高,bq25070自行降低了充电电流,你可以尝试用外部电源供电,把电压调低一点,如果可以维持充电电流,那么修改可以从加大芯片底部散热面积,适当降低充电电流,降低输入电压规格避免芯片过热。

  • 是的,如果不是因为输入导线太长造成实际的BQ2057输入端电压小于充电电压+Vdropout电压,那么建议重点请放在降低芯片的温度上,因为线性充电器的功耗可以用(vin-vcharge)*Icharge来大致估算,所以降低输入电压到Vdropout+Vcharge,同时将充电电流改小一点 ,此外芯片底部的散热pad有良好的与接地的铜箔焊接在一起,此时的芯片功耗和散热能得到大幅的改善,观察此时的芯片问对是否能维持在比较低的水平,设定的电流能否稳住。谢谢!