如果电路板用3.7V的单节锂电(3.6~4.2V)供电,但是板上的运放需要±12V供电。对于这个-12V,有合适降压芯片推荐吗?电路板的最大工作电流1A。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
楼主可以看下TPS65131,2.7~5.5V输入,输出可以达到正负15V(可配置),输出电流最大2A。
Hi
1A是指+/-12V负载各1A还是共1A(也就是各0.5A)?
Hi
真个设备的工作电流是1A, 是指输入得总电流是吗?,那就没有问题了。
12*0.5/0.9/3.6*1.1=2.0A 这个是算MOS的峰值电流,12V*0.5A是输出功率,除以0.9效率得到输入功率,除以最低输入3.6得到最大输入电流, 电感的ripple电流是最大输入电流的0.2倍(通常是通过这样来确定电感的),输入峰值电流是输入电流+0.2/2倍的输入电流,即1.1倍最大输入电流。
输入最大的峰值电流就是MOS的最大峰值电流,这个电流值是需要小于最小的MOS电流限制值1800mA的。
hi,
你的意思是+/-12V都输出1A吧?那么如Smith所说,输入电流需要4A左右,所以推荐+12V电源轨建议采用TPS55330,其参考设计可以参见TI在线仿真软件WEBENCH:webench.ti.com/。
-12V电源轨建议使用LMR25015,采用共地的负压输出结构(具体设计类似参考http://www.ti.com/lit/ug/snva363e/snva363e.pdf)。
您好,我从手册后面的图形来看,输出-15V时候的输出电流不能到达2A。如您这边说的,最大电流为2A,若是额定工作在-15V,1A情况下,对片子是否有影响呢