求推荐几款IC,开发的手持设备是单节锂电(3.5~4.2V)供电,需要3.3V的稳压输出,希望通过降压转换后,输出的电流Imax可以达到1A
因为电路板上还有其他值的电源(+10V、+5V)需要,若转换输出的3.3V电流太低,再做升压,那升压输出的电流就更低了
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,
根据您的需求,推荐您用webench工具进行选型,webench.ti.com.
我初步看了一下符合您要求的芯片还是很多的,诸如TPS62080等,但是不知道您对该款芯片除了输入输出要求等外是否还有其它的特别要求,所以您可以用webench工具试一下。
由于我是单节锂电输入(3.6~4.2V),我板上需要的电压分别有+3.3V +5V +20V +40V(可能+46V)-5V,而且+5v电源要求纹波极小
最后决定所有的电源都用电源IC从锂电得到,目前确定运放所需的±5V用TPS65131 纹波要求高的+5V单独用LM2733 +3.3V用TPS62020(TPs54317) +20V也用LM2733 +40V及以上的还在考虑中