我们有两块板卡用了TPS386596,A板卡上用了两片监测8路电压,这两片的reset信号是直接接到一起用了一个4.7k电阻,接入了一片SN74AHC1G08DBVR的输入,B板卡上用了1片监控四路电压,reset上拉4.7k,接入SN74AHC1G08DBVR。最近加工批次的两种板卡出现奇怪的现象。同一片TPS386596在A板卡上reset输出为低,换到B板卡上reset输出就是高了。A板卡上把后级SN74AHC1G08DBVR断开,reset也能抬高。但是把B板卡上的SN74AHC1G08DBVR换到A板卡上,reset信号仍为低,更换了另一个批次的TPS386596,A板卡reset输出为高。感觉像是不同批次的TPS386596有比较大的差异。这个问题芯片供应商还做了抛片,证明是TI生产的。reset为低时测sense1-4的电压都在阈值之上,sense1是3.15V,sense2-4都是0.425以上。