Other Parts Discussed in Thread: UCC3895
请问各位高手和专家,我正在用UCC3895做逆变项目,原理图参考设计参考TI的资料。UCC3895外接12.5V供电,用电流模式,EAP外接电阻分压电位为2.5V, 主电源接50V直流电,这时板子能正常工作,波形正常。但是主电源接交流220V整流得300V直流电,再UCC3895接12.5V时,UCC3895的VCC马上击穿.
本人是新手,请高人帮分析一下原因,谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
昨天我参考了论坛中一位朋友的建议,将UCC3895与每个UC27324之间加了一个下拉5K电阻,接220V(AC),再接辅助电源12.5V(DC),芯片没有击穿,但是空载时MOS管发热很快,我怀疑死区时间太小,DELA-B,DELC-D由原来的3K改为2.4K,Rads=10R,因为我设置UCC3895频率为最低频率89K,外部还有一个频率SYNC最高达到260K,但是这样接220V(AC)后,再接辅助电源12.5V(DC),UCC3895好象就损坏了。这个现象到底是什么原因引起的呢?
请TI的专业人士帮我分析一下。非常感谢。