Other Parts Discussed in Thread: BQ34Z110
TI技术支持:关于EV2300的校准顺序和方法想请教一下.
在开发铅酸蓄电池电量计时,电量计已经学习好了,但实际的测量精度总大于1%。大约在5%之内。我想误差大的原因大概是电压、电流和温度校准有问题
于是我使用EV2300对BQ34Z110进行校准。但是测量精度仍无改善。所以特请教以下几个问题,望不吝赐教!
1) 使用BQ34Z110的电量计计量20MAH左右的铅酸蓄电池的一般精度范围应该是多少?1%以内?2%以内?还就是5%以内?
2) 使用EV2300校准时,是先校准库仑计数器,再校电压、温度,最后校电流?正确的校准顺序是什么?
3) 校准电流时我在键入实际电流框里填入1000MA,按校准键后,在测量电流框里显示的校准后的电流总比键入的电流大10MA左右,为1010MA。如键入1500MA,则测量电流是1509或1510。不知道是为什么?我认为校准后的电流应该与键入的实际电流相同,对不对?
谢谢!