This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM338: 在设计基于LM338的电源电路时产生疑问

Part Number: LM338
Other Parts Discussed in Thread: LM317,

我在设计基于LM338的电源电路时参考了LM317的电路设计,试图采用一个PNP型三极管提供大部分电流,以减小LM338的产热,请问这样设计安全且科学吗?

  • HI

        我觉得是没有问题的,但是这个并非TI参考电路,建议实测电路验证。

        同时不建议这样设计,LDO不建议用在大压差高电流即高功耗时,如上电路的效率只有33%,而且功耗很大。

        建议用DC/DC, 一般采用降压芯片效率都可能达到90%以上,甚至95%。

  • 非常感谢您的及时回复,请问您对输出电压要求5~10V,输出电流~1A低纹波应用场景下的DC-DC芯片有什么建议的选型吗