Other Parts Discussed in Thread: TPS62150, TPS62060, TPS62130
本人刚开始使用DC/DC电源芯片,任务输入为12V,需要产生5V、3.3V、1.8V、1.2V、2.5V电压的二级电源。目前方案是使用1颗TPS62150由12V产生5V,再使用3颗TPS62060由5V分别产生3.3V、1.8V和1.2V,使用TLV70225由3.3V产生2.5V电压。
焊装好后测试12V输入电流为0.22A(输入功率2.7W),即使按效率100%计算,5V的输出电流也就0.54A,而TPS62150的额定输出电流为1A,可是不知为什么每次工作几分钟后TPS62150就会烧毁,烧毁后输出和地短路,使用2块板子各烧了2片现象一样。单独使用电子负载拉TPS62150的输出1A没有问题。请各位大神帮忙分析一下哪里的问题,怎么改进,难不成是因为开关频率耦合了?谢谢!