This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC27211: 做逆变驱动器,输入SPWM波,上管吞波。输出方波,而不是SPWM。

Part Number: UCC27211

个人觉得影响因素:QG RG CBOOT C滤波 当然还有LAYOUT,

SPWM输出正常情况:MOSFET:FR24N15D Vdss=150V Id=24A RDSON=95mOHM QG=30NC Cboot=100NF C滤波=100NF Rgate =47ohm.(就一次) MOSFET供电17V左右 VDD=12V

因为经常炸管,更换MOS又是吞波,SPWM出不来。计算CBOOT=23NF左右,还是有问题。Rgate算出来是负的,应该算错了。不知道该怎么解决,之前还试过输出的确是SPWM但是是抬高电平的。附图就是输出不对的信号。