Part Number: BQ40Z80
Other Parts Discussed in Thread: GPCCHEM
updata state = 0x05 ,放电后静置阶段 VOK没有被置0,无法进行下一步。附件log,请求帮忙分析一下原因和对策,感谢。
6S电芯,单芯充电电压4.4v,放电截止电压3.2。log-20230318.log
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,请参考下面文档4. 电量计 Golden Learning 易错分析
Chemistry ID selection tool, rev=2.54 Configuration used in present fit: ProcessingType=2 NumCellSeries=6 ElapsedTimeColumn=0 VoltageColumn=1 CurrentColumn=2 TemperatureColumn=3 Best chemical ID : 1528 Best chemical ID max. deviation, % : 2.19 Summary of all IDs with max. DOD deviation below 3% Chem ID max DOD error, % Max R deviation, ratio 1528 2.19 0.44 2571 2.21 0.68 3991 2.23 0.83 2456 2.3 1 2620 2.34 0.79 5347 2.38 0.69 2166 2.42 0.65 3621 2.42 1.57 3897 2.43 1.11 1752 2.44 1.07 2994 2.45 0.88 3972 2.47 0.87 3878 2.49 0.65 2707 2.5 1.78 2220 2.5 1.01 5657 2.5 0.63 2699 2.5 0.92 3955 2.5 2.72 1786 2.51 1.91 1621 2.52 0.78 3641 2.52 1.43 2298 2.53 0.7 900 2.53 0.7 1657 2.53 1.05 3952 2.54 1.11 2212 2.54 1.04 5580 2.56 0.67 1637 2.56 0.72 1660 2.58 1.41 2717 2.59 0.61 5653 2.59 0.79 3994 2.6 0.93 2389 2.6 0.63 2167 2.6 0.67 2236 2.6 0.73 7114 2.6 0.72 3950 2.6 1.42 579 2.6 0.73 3989 2.61 0.77 2247 2.61 1.28 2464 2.61 0.63 2235 2.61 0.66 2668 2.62 0.93 3578 2.62 1.56 2633 2.62 0.69 536 2.62 0.77 3940 2.62 0.89 2559 2.62 0.97 2473 2.63 0.77 2221 2.63 1.04 5101 2.63 0.74 1782 2.63 0.83 2438 2.64 1.59 2766 2.64 0.69 3803 2.65 1.74 1791 2.65 2.03 1808 2.65 1.05 2485 2.65 1 3851 2.65 0.95 3938 2.66 0.77 3880 2.66 0.88 2839 2.66 0.59 2767 2.66 0.73 3706 2.67 0.8 1744 2.67 0.86 2739 2.68 0.79 1987 2.69 0.88 2635 2.69 0.8 3951 2.69 1.4 2352 2.7 0.72 1478 2.7 1.35 2823 2.7 0.6 1848 2.7 1.46 1818 2.7 1.56 1801 2.7 0.7 2826 2.7 0.63 2223 2.7 0.79 5373 2.7 0.63 5143 2.71 0.67 1534 2.71 0.9 3314 2.71 1.81 2643 2.71 0.63 1432 2.71 1.21 2838 2.71 0.62 1408 2.71 0.97 2706 2.71 0.58 3980 2.71 0.87 1693 2.72 1.5 5677 2.72 0.63 5165 2.73 0.75 2999 2.73 1.02 2724 2.73 1.44 1600 2.74 1.28 1799 2.74 1.74 2275 2.74 0.79 1616 2.74 0.98 2928 2.75 0.76 3829 2.75 0.71 3934 2.75 0.71 3843 2.75 1.34 2222 2.75 0.94 1725 2.75 1.26 3901 2.75 1.46 3977 2.76 0.87 2231 2.76 0.83 3946 2.76 1.12 3827 2.76 2.18 1822 2.76 0.86 2230 2.76 1.32 1796 2.76 0.9 1476 2.76 1.74 2726 2.77 0.8 2941 2.77 0.71 2549 2.77 0.71 575 2.77 0.61 1663 2.77 0.96 2217 2.77 1.09 5589 2.77 0.65 2660 2.77 0.67 1721 2.78 1.35 2927 2.78 0.61 501 2.78 0.76 1787 2.78 0.71 2810 2.78 0.65 5157 2.78 0.71 1897 2.79 0.88 2780 2.79 1.18 5502 2.79 1.37 5484 2.8 0.61 5357 2.8 0.6 2873 2.8 0.62 1910 2.8 0.88 1481 2.81 1.14 3963 2.81 1.73 2490 2.81 0.79 1683 2.81 1.08 3509 2.81 1.83 1920 2.81 1.39 2497 2.82 0.85 2198 2.82 0.87 5462 2.82 0.69 2207 2.82 0.74 3840 2.82 0.87 1584 2.82 0.79 3597 2.82 1.62 2913 2.83 0.62 5198 2.83 0.67 5869 2.83 0.89 3995 2.83 0.89 1723 2.83 0.94 3920 2.83 1.37 502 2.83 0.71 5398 2.83 0.61 3905 2.83 0.75 2867 2.83 0.65 2907 2.83 0.64 5138 2.83 0.95 5172 2.83 0.67 3917 2.84 1.28 1506 2.84 0.83 7056 2.84 1.04 2977 2.84 0.64 1986 2.84 0.93 5306 2.84 0.63 1709 2.85 1.11 2344 2.85 0.62 5468 2.85 0.64 7046 2.85 0.69 2704 2.85 0.79 3802 2.85 1.15 2569 2.85 0.87 1845 2.86 1.41 1514 2.86 0.93 3783 2.86 1 2784 2.86 0.62 1682 2.86 2.19 2917 2.86 0.67 5305 2.86 0.66 2914 2.86 0.63 2786 2.86 0.79 2210 2.87 0.83 5158 2.87 0.91 5900 2.87 0.63 1409 2.87 1.23 5174 2.87 0.62 3716 2.87 1.24 2383 2.87 0.77 534 2.87 0.65 3998 2.87 0.84 7004 2.87 0.87 2299 2.87 0.9 2577 2.87 0.77 2785 2.88 0.66 509 2.88 0.94 3541 2.88 1.36 5336 2.88 0.61 5564 2.88 0.73 1690 2.88 0.96 1670 2.88 0.96 3689 2.88 2.08 1700 2.88 1.21 1849 2.88 1.41 5136 2.88 1.14 5210 2.88 0.64 1623 2.88 1.23 540 2.89 0.66 2723 2.89 0.77 5507 2.89 0.61 1635 2.89 1.01 5197 2.89 0.61 2611 2.89 0.71 2985 2.89 0.9 1696 2.89 1.36 5546 2.89 0.86 5123 2.89 0.62 2226 2.89 1.17 2932 2.9 0.63 5173 2.9 1.14 2173 2.9 0.75 2775 2.9 0.82 2522 2.9 0.89 2836 2.9 0.67 5328 2.9 0.91 2920 2.9 0.81 5125 2.9 0.65 3939 2.9 0.75 2532 2.9 1.05 7050 2.9 0.6 5970 2.91 0.72 5685 2.91 0.71 5102 2.91 0.65 2665 2.91 0.63 558 2.91 0.64 3945 2.91 0.89 1650 2.91 0.98 2719 2.91 0.75 1980 2.91 0.82 5735 2.91 0.41 1622 2.91 0.78 2253 2.91 0.72 2778 2.91 0.61 5195 2.91 0.62 2896 2.92 0.73 1836 2.92 1.01 1598 2.92 0.62 5335 2.92 0.71 3978 2.92 1.38 517 2.92 0.63 5356 2.92 0.72 1990 2.92 1 5466 2.92 0.71 5229 2.92 0.6 5806 2.92 0.8 5423 2.92 0.74 2604 2.93 0.65 5560 2.93 0.63 5824 2.93 0.89 1793 2.93 1.15 2523 2.93 0.87 1900 2.93 1.5 5212 2.93 0.56 5823 2.93 1.84 2898 2.93 0.79 5384 2.93 0.81 1614 2.93 0.9 2395 2.93 0.99 2296 2.94 0.84 1713 2.94 1.37 2472 2.94 1.01 7024 2.94 0.77 2793 2.94 0.71 1420 2.94 2.09 3983 2.94 1.28 3857 2.94 1.63 2113 2.94 2.09 1385 2.94 1.54 2515 2.94 0.94 2829 2.94 0.89 5988 2.94 0.63 596 2.94 1.28 1979 2.94 0.89 5406 2.94 0.63 2511 2.94 0.93 5296 2.94 0.55 7060 2.95 0.65 5480 2.95 0.65 2850 2.95 1.13 5967 2.95 0.72 1655 2.95 0.93 5332 2.95 0.61 5460 2.95 0.64 560 2.95 0.61 1468 2.95 0.94 5242 2.96 0.71 1735 2.96 1.35 5997 2.96 0.65 3613 2.96 1.21 1904 2.96 2.55 1486 2.96 1.14 5240 2.96 0.74 5863 2.96 0.65 5151 2.96 0.73 7089 2.96 1.72 5579 2.96 0.66 1414 2.96 1.54 1746 2.96 1.15 5866 2.96 0.72 5798 2.96 0.64 5149 2.96 0.77 5633 2.97 0.99 1978 2.97 0.96 3688 2.97 0.84 2889 2.97 0.61 2940 2.97 1.32 2441 2.97 1.31 3761 2.97 2.11 2614 2.97 0.93 2805 2.97 0.68 1410 2.97 1.03 2644 2.97 0.64 3676 2.97 1.03 5596 2.97 0.77 3750 2.97 1.51 2674 2.98 0.65 5439 2.98 0.63 2687 2.98 0.76 5216 2.98 0.8 1803 2.98 1.68 1883 2.98 1.64 523 2.98 0.87 1502 2.98 1.23 2492 2.98 0.63 5684 2.98 0.8 5445 2.98 0.7 1826 2.99 1.18 5337 2.99 0.65 2458 2.99 0.63 2270 2.99 0.68 5524 2.99 0.64 2613 2.99 0.74 544 2.99 0.6 1736 3 0.94 5551 3 0.76 587 3 0.62 1691 3 1.22 1656 3 1.44 7055 3 0.69 2243 3 0.74 3845 3 2.9 Max. deviations for best ID is within recommended range. Chosen best chemical ID is suitable for programming the gauge. Selection of best generic ID for ROM based devices like bq274xx Device / Family #1 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 3142 bq27421-G1D: 4.4V LiCoO2 4.74 354 bq27411-G1C: 4.35V LiCoO2 5.34 312 bq27421-G1B: 4.3V LiCoO2 8.12 128 bq27421-G1A: 4.2V LiCoO2 13.78 Best generic ID 3142 Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family. Device / Family #2 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 354 bq27621: (ALT_CHEM2) 4.35V LiCoO2 5.34 1210 bq27621: (ALT_CHEM1) 4.3V LiCoO2 8.9 1202 bq27621: (default) 4.2V LiCoO2 15.19 Best generic ID 354 Warning: Deviation for best generic ID is above recommended level for this device / family. Consider using another device, flash based gauge or RAM programming of custom ID. Device / Family #3 Generic Chem ID Device/ Voltage/ Chemistry max DOD error, % 3142 bq27426: (ALT-CHEM2) 4.4V LiCoO2 4.74 3230 bq27426: (default) 4.35V LiCoO2 5.34 1202 bq27426: (ALT_CHEM1) 4.2V LiCoO2 15.19 Best generic ID 3142 Max. deviations for best generic ID is within recommended range. Please chose this ID in your device configuration or device family.