Other Parts Discussed in Thread: LM2575, LM25118
输入:8~40V,输出1:3.3V1A,给DSP及逻辑电路用,输出2:+15V1A,给外围一个传感器供电,同时做运放正电源,输出3:-15V0.1A,运放负电源,不隔离,但是体积高度敏感,希望越小越好,板子上只有比LM2575(全部表贴)的电路大一点的地方,)同时不希望自己绕变压器(水平较差,试了几次没成功),能用市场直接采购的元件搭起来最好。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
总共有20W输出,电源设计最主要就是变压器的设计了,如果要用现成的,不太显示,买个电源成品还现实一点。
总共有20W输出,电源设计最主要就是变压器的设计了,如果要用现成的,不太显示,买个电源成品还现实一点。
这成本可不低啊.得升降压电路了.不要变压器可以,买成品电感就行
但你这面积实在太憋屈了.
要不就搭立体式的?板子上再插卡解决?
感谢上面所有回复,我接手这个电路以前是用LM2575加一个表贴电感降到5V,然后用TPS767D318降到3.3和1.8V给DSP供电的电路,现在想把原电路直接降到3.3,但是要加一个传感器和输出运放的供电,所以麻烦比较大,板子的反面倒是可以贴器件,而且地方大多了,但是高度不能超过2mm,因为离底壳只有3mm的距离,我按2楼的建议查了一下,LM25118评估板上的那个电感一下就把元件面的地方全占了,肖特基二极管根本排不下,而且这个板子高度还有限制,大约16mm到17mm左右,虽然成本控制可以放得比较宽,可是还是太困难了。
另外,变压器方案试过,但我不是专业做电源的,所以对变压器的设计十分头疼。单端反激,推挽,半桥都试了一遍,结果是烧了十几个管子后只好放弃。