This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM3478升压电路

Other Parts Discussed in Thread: LM3478, TL494

   我用TI的LM3478资料做3.7V升到5V,且电流要达到2A,但测试时供电就过流,并且我看资料中说通过改变7脚的电阻来改变频率,并且频率在1kHZ-1MHZ,但我们的频率一直不变只有50多HZ,想问下是什么原因?求解!

  • 如果开关频率不能达到通过FA电阻设定的值,检测供电以及接地良好的情况下,建议你换一个芯片,按照你描述的现象,极有可能芯片内部的晶振模块被损坏了,这个50多HZ的开关频率是没有办法满足boost电路工作需求的。谢谢!

  •    谢谢你的解答, 但我做了两块板子都用新的芯片,都是供电就过流,并且两次电流值的大小都不一样。还有我在用LM3478和TL494时遇到相同的问题,就是如果直接给它们供工作电压就过流,但是从工作电压以下慢慢调到工作电压时就不过流,但电路还是没有正常工作。

  • 您好,请确保电路焊接没有问题,可以参考datasheet完成设计,建议上传电路原理图,谢谢