This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Johnsin Tao你好!

Other Parts Discussed in Thread: LM3466, TL4242

附件为AT070TN92的规格书!!麻烦你了!

AT070TN92 P(V02)_0622.pdf
  • 在显示屏AT070TN92的规格书中并没有提到屏幕中是否有控制LED的芯片或者调光灯电路, 但是明确有将LED+接9.3V/180mA(典型值), 而并不其他信号控制,则如果屏幕中背光控制只是串联的LED灯,则可以通过LED-( CN的脚3/4)来控制亮度,  例如LM3466 :www.ti.com.cn/.../lm3466.pdf 就可以连接到LED-作为定电流的设计。

    (我正在寻找其他诸如LM3466且带调光功能的更加LED驱动芯片,LM3466如要调光还需要额外串联MOS到LED串上)

    其次您可以问一下LCD显示屏厂商,问一下他们是否有推荐的LED驱动。

  • 如果您有找显示屏厂商确认,LED+和LED-在显示屏中并无其他控制电路,只是接背光灯,则可推荐使用TI的TL4242: www.ti.com.cn/.../tl4242.pdf , TL4242比较适合于您的应用, 芯片Pin脚I接9.3V, Pin脚Q接LED+, REF接LED-, 电流180mA,则设计电阻Rref=177mV/180mA=0.98ohm, PWM脚用于亮度调节。

    或许您需要将9.3V设计略微再高一点,原因是TL4242的I脚和Q脚之间存在Vdrop, 在180mA电流下估计在0.3V左右, 这个在调试中要注意。