This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65251第一路输出1.2V异常



你好,我用第一路作为1.2V输出,3A输出电流。上电后发现无论如何加大输出那段的电阻,输出电压一直处于1.002V,测量了一下FB1端电压,发现是0.68V0.8,而不是0.8V。同时LX1的输出波形也不是占空比为50%的方波。类似于尖峰波。请问是什么回事呢?

  • 第三路输出5.5V却是正常的。需要说明的是第一路空载,第三路带负载。

  • 能否将您的电路图附件上来看看,并说明一下输入电压,LX1反应的是buck1的占空比,近似于D= 输出电压Vo/输入电压Vi ,而输入电压需大于4.5V, 所以占领比会小于40%,不会达到50%.

    请先确认一下BST1的电容(可新换一个或者与第三路对调), charge pump的电容异常会导致buck上臂的MOS驱动异常。

  • 输入电压是12V,另外我如果要使能三路输出电压,那这个使能电压是多少?比如我先上电1.2V,然后到1.8V,在到3.3V,那么EN1,EN2 ,EN3要加多大的使能电平;我发现加了1.6V的电压,三路都没输出。

    另外空载是不是输出会异常。

  • 输入电压是12V,另外我如果要使能三路输出电压,那这个使能电压是多少?比如我先上电1.2V,然后到1.8V,在到3.3V,那么EN1,EN2 ,EN3要加多大的使能电平;我发现加了1.6V的电压,三路都没输出。

    另外空载是不是输出会异常。

  • EN的门槛电压是1.55V, 所以您加1.6V时要注意实际到芯片脚的电压是否高出1.55V(不同的芯片还可能有小的差异), 不建议采用比较margin的1.6V作为使能电压,建议采用高一点的。其次需要说明的是,即便不增加使能电压给EN,因为EN在芯片内部通过1M电阻上拉3.3V,三路也会慢慢启动。

    要控制1.2V/1.8V/3.3V的时序,可以在EN处增加容,即便同时给电压到3个EN, 而会因为电容不同造成不同启动时序,每增加1nF电容,可造成1.67mS的延时启动。例如1.2V不加电容,1.8V增加2.2nF, 3.3V增加4.7nF, 可以使得1.2V启动后3.67秒1.8V启动,再过4.17秒3.3V启动。

  • 两外空载不会造成输出电压异常。电路方面参考datasheet或者EVM板指导说明即可。