Other Parts Discussed in Thread: TPS5430, TPS54360, TPS54260
能否利用TPS5430输出大于负8V的电压,或者求推荐开关频率和TPS5430一个级别或者比5430更高的DCDC负电压输出的芯片?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
应该是可以的,参考一下这个应用
用此芯片可以输出,不过你要看清楚你的正负极,其实就是把地当做高电平,把输出当地,即可。不过要注意:如果给TPS5430供电的电源接几路非隔离电路,如果几路中有共地现象,之前实现负压的方法就不可行了,谢谢,欢迎补充指正。
Hi
只要Vin(正电压)对Vout(负电压)的电压不要超过36V即可,也就是说要看看你的Vin最大电压,如果Vin电压不大可以产生-8V的负电压。
或者你可以选择TPS54260/TPS54360等芯片,他们的耐压是60V.