Other Parts Discussed in Thread: BQ2057C
BQ2057C的TS脚通过热敏电阻反馈的电压怎么和内部V(TS1)和V(TS2)扯上关系的。手册没有给出V(TS1)和V(TS2)对应的电压值 ???
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: BQ2057C
BQ2057C的TS脚通过热敏电阻反馈的电压怎么和内部V(TS1)和V(TS2)扯上关系的。手册没有给出V(TS1)和V(TS2)对应的电压值 ???
您好,V(TS1)和V(TS2)对应的电压值是随着VCC变化而变化的,因此不可能给出具体电压值。
但是datasheet给出了V(TS1)和V(TS2)所占VCC的比例。热敏电阻同样分VCC与VSS的电压,通过比较可以实现温度监控。
嗯,是我没看懂手册,谢谢您了!还有个问题就是:我要电池充到3.8V就停止充电,应该如何处理呢??
您好,我能问一下您为什么要让电池充电3.8V停止充电吗,谢谢。
您好,因为充电电池18650最高电压是3.8V啊!充满超过3.8V就不能冲了!
您好,根据您的描述,可以参考datasheet,图7(图8)设定稳压模式电压,希望有帮助到您,谢谢。
是的,但是根据datasheet(图)流程图来看,最后充满的条件是V(BAT) >V(RCH),但是datasheet第六页给的V(RCH)是100mV,确实没怎么搞懂,望解释,谢谢您了!
你好,
V(RCH)是指电池recharge的门限电压,数据手册中V(RCH)的典型值为Vo(REG)-100mV。是指电池电压充到Vo(REG),一个充电周期结束后,若电池电压跌落100mV,charger会自动重新充电。
一般常用的锂离子电池满充电压为4.2V或4.35V。若为3.8V可能是其标称电压。当然充电的电压的最终设置要根据您选用电池的数据手册来确定。若要设置电池的充电截止电压为3.8V,bq2057C是不能达到这一要求的,其充电电压设置为4.2V(典型值)。