Part Number: TPS61196-Q1
Other Parts Discussed in Thread: TPS61196
参考原理图,我司6并17颗串LED灯板采用TPS61196驱动,设置最大单路200mA,总输出52v,1.2A最大,正常使用700mA左右,目前发现烧毁IFB脚后Fault置高不可点亮LED问题,同时也有发现肖特基二极管烧毁D6问题。怀疑保护设置不到位,所有坏掉驱动IC板对应的LED灯板都是好的,没有短路问题,工作正常。目前设置13.3A保护电流应该太高,后续修改。另外,关于LED短路保护,在芯片数据手册低16页这样描述: “If any IFB pin voltage exceeds the threshold (VLED_SHORT)” 就是说任何一个IFB管脚的电压超过VLED_SHORT。我们设置的VLED_SHORT是11.88v,而我们实测的低PWM占空比时,IFB是12.7v超过了VLED_SHORT,但没有保护,所以认为对该功能的理解不到位,望指点之所以提出该问题是因为更严重的问题:驱动IC正常工作时,或开启后发现灯不亮,测试发现我们肖特基二极管和IFB pin脚内部都有烧短路的情况发生,所以在找原因时怀疑到led短路保护功能