Other Parts Discussed in Thread: UC3825, UCC28251, TIDA-00173
你好!我们有一个超宽输入DC200-1000V,输出为DC48V/5A的电源项目,可靠性要高,对效率暂时不要求,需要有输出过压,短路等保护功能,用于光伏上的。为了提高变压器的利用率,适应宽电压输入,我们准备用半桥拓扑结构。请问一下TI工程师:对于这种超宽电压输入电源,你们有什么意见?有没有比较好的驱动IC推荐?谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Other Parts Discussed in Thread: UC3825, UCC28251, TIDA-00173
你好!我们有一个超宽输入DC200-1000V,输出为DC48V/5A的电源项目,可靠性要高,对效率暂时不要求,需要有输出过压,短路等保护功能,用于光伏上的。为了提高变压器的利用率,适应宽电压输入,我们准备用半桥拓扑结构。请问一下TI工程师:对于这种超宽电压输入电源,你们有什么意见?有没有比较好的驱动IC推荐?谢谢!
输入电压到1000V,对于开关器件和驱动电路的选择来说是比较困难的,开关管一般只有IGBT或者SiC的MOSFET,驱动也只能采用变压器隔离驱动或光耦,很难找到合适的集成驱动器。
采用半桥电路能够降低变压器原边的应力,但需要两只钳位电容,在类似的应用中也有见到采用双管正激的,可以参考一下。
你好!我有类似的需求,输入端AC100-600V,输出28ACV,25W。可以与你交流吗?
Hi Xuan yi,
AC100-600V, 25W应用可以参考TI参考设计TIDA-00173,谢谢
Regards,
Patrick
Hi,Patrick Zeng
我研究一下你建议参考的设计,谢谢!
Best Regards