This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28070高温限功率

Other Parts Discussed in Thread: UCC28070

你好!

   我们公司在使用汽车级UCC28070设计的PFC电路中,发现在高温环境下(85°C)UCC28070会进入限功率模式,具体表现为输出电流下降,请问是怎么回事呢?

  •        UCC28070带有电流限制功能“Peak Current Limiting” 您在可以在85℃环境下测试PKLMT的电压(有VRef分压得到)与CSA/B波形的最高电压,如果这个时候比较接近或者CSA/B已经出现高出PKLMT电压,则已经产生过电流限制,您可以通过修改PKLMT的分压电阻使得PKLMT电压再略微高一点点来避过这个比较极限的状态85℃。

  • 你好,请问你所带负载的特性是什么?一般调试PFC输出会考虑带CC或者CR的负载。

    1.如果带CC的负载理论上不会出现进入限功率模式后电流下降的情况

    2.如果是CR的负载在减小电阻的时候输出电压会被拉下来引起输出电流下降,那么请考虑是不是:a.芯片达到了最大占空比而限功率;b.电感的负温度特性使峰值电流增大触发芯片的"peak current limit"。