90V~230V转正负18V输出,以及正9V输出,带载能力各自有2A就可以(100W),效率有80%就可以,最好纹波低一些,要是能有主动pfc更好。
多谢各位。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
PFC用UCC28051/ UCC28019A, PWM芯片用UCC28600.
TI没有提供完全符合您设计参数的案例或者参考设计,下面是TI的120w设计,你可以参考,这个输出是19.4V, 你需要多一个绕组出来做其他电压,PFC可以沿用。
http://www.ti.com.cn/general/cn/docs/lit/getliterature.tsp?baseLiteratureNumber=sluu256&fileType=pdf