Other Parts Discussed in Thread: BQ24133, BQ24171
你好,根据BQ24133数据手册,它是支持1-3芯的锂电池充放电。那么BQ24133支持3芯2并的锂电池组充放电吗(锂电池的电压是11.1V)?还是说只支持3芯(1并)的锂电池呢(锂电池的电压是11.1V)?。谢谢~
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
你好
请教一下,3芯2并是什么意思呢?需要注意的是BQ24133的锂电池电压是支持标准电芯1-3节串联,即输出电压只有4.2V, 8.4V, 12.6V。看上去你的是11.1V,所以是非标准电芯,这样你需要使用可调输出电压的充电芯片,如BQ24171。
http://www.ti.com.cn/cn/lit/ds/symlink/bq24171.pdf
你好,3芯2并指的是 3 series 2 parallel (电池组的结构是 3串联 2并联),电池的标称电压是11.1V。BQ24133支持这样的电池充放电吗?
可以的,你说的11.1是一般锂电池标称电压3.7V X3,但通常充电器是以cv电压乘以串联节数,比如4.1、或者4.2或者4.35 乘以3来描述的.
并联以后容量加倍,所以你需要的cc电流加大,看看你电池的规格书中推荐的充电比率是多少,2并就加倍,再 检查一下BQ23133是否能支持这个电流。
您好,请问你的电池是一个自带电池管理,保护的电池包么?充电上限电压是多少?容量是多少?
对于充电管理芯片来说,能设置的就是充电电压和充电电流,只要电压和电流够用,不关注是多少并联和串联。
谢谢。