Other Parts Discussed in Thread: UCC28019, UCC28180, UCC28070, UCC28050, UCC28061, UCC28063, UCC28060
85~264宽AC输入,385Vdc输出,600-1000w(待定), 满足这样条件的PFC芯片求推荐
谢谢!
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
UCC28180:
UCC28019
8 引脚持续传导模式 (CCM) PFC 控制器
The UCC28019 8-pin active Power Factor Correction (PFC) controller uses the boost topology operating in Continuous Conduction Mode (CCM). The controller is suitable for systems in the 100 W to >2 kW range over a wide-range universal ac line input. Startup current during under-voltage lockout is less than 200 µA. The user can control low power standby mode by pulling the VSENSE pin below 0.77 V.
Low-distortion wave-shaping of the input current using average current mode control is achieved without input line sensing, reducing the Bill of Materials component count. Simple external networks allow for flexible compensation of the current and voltage control loops. The switching frequency is internally fixed and trimmed to better than 5% accuracy at 25°C. Fast 1.5-A gate peak current drives the external switch.
Numerous system-level protection features include peak current limit, soft over-current detection, open-loop detection, input brown-out detection, output over-voltage protection/under-voltage detection, a no-power discharge path on VCOMP, and overload protection on ICOMP. Soft-Start limits boost current during start-up. A trimmed internal reference provides accurate protection thresholds and regulation set-point. An internal clamp limits the gate drive voltage to 12.5 V.
具体参选信息,可以点击下面的网址http://www.ti.com.cn/product/cn/UCC28019
可以试试UCC28070,交错CCM模式的,效率高,散热好,功率再大点也不是问题
UCC28019、UCC28180、UCC28070、UCC28050、UCC28061、UCC28063等等一些都可以看看的。http://www.ti.com.cn/sitesearch/cn/docs/universalsearch.tsp?searchTerm=UCC28#linkId=2