This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25172EVM: BQ25172DSGR idle charge current

Part Number: BQ25172EVM

When BQ25172DSGR without connector Ni-MH battery for charge. The BQ25172DSGR idle current is about 250mA.

Is it correct? it look is so high.

And when connetor battery about 4.0V it do not go to charge status,. Why? the Ni-NH battery full voltage should be over 4.0~4.4V. it is not full charge.