Other Parts Discussed in Thread: TPS40210, TPS40211, CSD18502KCS
电路是按照WEBENCH设计图TPS40210导出到AD做的,实际使用芯片TPS40211,两者的FB电压要求不一样所以改了反馈电阻(如电路图中的Rfb1)。
MOS管使用的IRF840(????不知道是不是由于导通电阻太大了,反正很烫啊啊啊啊)
要求:输入5~14V,输出为24V,输出电流1.5A
焊完电路,测试时发现:使用固定5V输入的时候,MOS管非常的烫,输出电压为;
使用稳压源的输入的时候,设定为大于5V等数值时,一按下输出,就会固定输出在4.2V左右,输出的电压从17.3V开始上升到22V左右不再发生变化
求大神们解答呀~~~~