我参照BQ24650的评估板的电路设计了一个类似的电路,由于元件的限制,将里面的Q1和Q2均换成了手头有的IRF3205,以及上面的肖特基均换成了IN5822,现在的问题是充电的引脚VOUT根本就不能输出(输出带不了负载和输出电压完全不对)。参照评估板的用户手册2.6和2.7我记录了测量结果,我使用的VIN是20.8V。1、(参照用户手册2.7.1)我将电路不接负载悬空时,将CE接高电平有,VSYS为20.68,VOUT为2.8,VREF为3.3,REGN为2.61;2、(参照用户手册2.7.2)我将电路不接负载悬空时,将CE接低电平有,VREF为3.3V,REGN为4.35,VOUT为0.79。这就很不对了。我仔细检查了电路,发现电路,基本和典型电路以及评估板的电路类似。仔细查看芯片手册,也没有发现什么可以调试的地方了。请问一下究竟是哪里出了问题。为什么不能输出正确的结果?