Other Parts Discussed in Thread: LM2576, TPS54233, LM22670
想找个低频率DC/DC,宽压输入(9-24V),固定5V输出,输出电流2A,纹波电压为30mv,之前的方案是NS LM2576,想找个可以替代此料件的IC,请帮忙推荐,主要是不用很复杂,价格在2美元以内.
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
推荐的替代芯片有TPS54233: 见EVM设计, www.ti.com.cn/.../slvu264.pdf 电路比较LM2576略微复杂,但是有参考设计,同时价格也会便宜很多。
Ember, 你好,为什么要替换LM2576?使用起来遇到什么问题吗?因为LM2576使用起来比较简单,方便。找低频率DCDC是不是因为遇到EMI问题?如果真是EMI问题,并不一定完全需要降低频率来解决的
Hi Jeff,你好,更换LM2576的原因:1.LM2576推出应该有好几年了,是否有LM2576的更新产品,毕竟现在的工艺也已经提高了许多.2.就是之前用LM2576发现纹波电压大概有40mv左右,而我们的系统要求纹波电压最好是在30mv以下.
找低频率的DC/DC是因为系统的模拟信号为1MHz左右,在选DC/DC的时候我会尽量选低频的.所以请帮忙推荐是否有可以替代的料件,谢谢!
LM22670 is OK.是SVA第5代的产品,工作频率可调,满足对频率调整的特殊应用。是目前我们比较推荐的一颗IC。有PSOP-8和TO-263Thin的封装