This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76930: 7串原理图

Part Number: BQ76930
Other Parts Discussed in Thread: BQ78350, BQ76200,

使用BQ76930+BQ78350做7串的方案(MOS高侧控制,使用BQ76200驱动),目8816.Schematic Prints.pdf前前端电压无法采集,后端无法通讯;PEGOUT输出电压0.6V;

  • 您好,正在查询,稍后回复。

  • 您好,In the external P-Channel FET balancing circuitry, the diodes are connected wrongly. The anode should connect to the gate of the FET and not after the gate resistor.



    Typically N-Channel FETs are used for external cell balancing as these are more robust for random cell connection. More details are explained in Section 10 Random Cell Connection – Within Limits of the bq769x0 Family Top 10 Design Considerations.

    I suggest they look at TIDA-01093 reference design for P-channel external balancing connections.

    TIDA-00792 reference design exhibits the BQ76200 high side driver and this design is the closest to the customer's design. Did they look at this design before? 

    I suggest you first detailly look at these designs.