This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPIC74100-Q1使用疑问

Other Parts Discussed in Thread: TPIC74100-Q1, BQ24210

芯片TPIC74100-Q1有两根5V电压,Vout和5Vg,请问这两根引脚有什么区别吗?

  • Hi ChengGuo,

    从芯片功能上来说:

    1. 5Vg的输入是Vout,所以,有Vout才有5Vg。由于内部MOSFET导通电阻,5Vg的电压要比Vout略低。导通电阻典型值135m Ohm,您可以通过负载电流进行计算。规格书标称最大400mA。在计算Vout最大负载电流的时候,需要将5Vg的负载电流叠加到Vout的总负载电流中。

    2. 5Vg和Vout通过一个内部MOSFET隔开,这个设计提供了a. 单独使能控制5Vg。b.5Vg瞬时限流功能。

    3. 当Vout小于4.65V(RESET置位信号阈值),5Vg会通过内部MOSFET被直接关断。

    谢谢。

  • Hi Amoeba,

    如果TPIC74100-Q1后接BQ24210的话,应当接5Vg吗?还是Vout?如果接5Vg,那么Vout怎么处理?同样的接Vout,5Vg如何处理?

  • Hi ChengGuo,

    请问是车载应用嘛?为何需要充电?

     

    1. 如果TPIC74100-Q1后接BQ24210的话,应当接5Vg吗?还是Vout?如果接5Vg,那么Vout怎么处理?同样的接Vout,5Vg如何处理?

    如果TPIC74100-Q1后端接BQ24210,那么,BQ24210 VBUS应该接的是Vout。因为TPIC74100-Q1芯片规格书给出的1A负载电流能力是针对Vout来说的,5Vg无法提供那么大的负载电流。如果您不需要使用5Vg,那么,您可以直接使用5Vg_ENABLE关闭5Vg,将该引脚接地。只要该引脚电压低于2V,5Vg理论上是关闭的。5Vg可以悬空,最好预留一个电容的焊盘接地。

     

    谢谢。

  • Hi Amoeba,

    是使用在能源收集方面,前端输入为0.1-18V。

    刚在数据手册里看到这样一段话。

    最后一句提到开关稳压器在V(driver)低于5V的时候不会开始。请问TPIC74100-Q1的启动电压多少?

  • Hi Amoeba,

    使用在能源收集方面,前端输入为0.1V-18V,0.01A-0.3A

    这样是使用Vout好,还是5Vg呢?

    刚在数据手册里看到这样一段话。

    最后一句提到开关稳压器在V(driver)低于5V的时候不会开始。请问TPIC74100-Q1的启动电压多少?

  • Hi ChengGuo,

    1. 这样是使用Vout好,还是5Vg呢?

    使用Vout.

    2. 最后一句提到开关稳压器在V(driver)低于5V的时候不会开始。请问TPIC74100-Q1的启动电压多少?

    虽然TPIC74100支持最小1.5V的输入电压,但是在启动瞬间,至少保证输入要能等于大于5V工作1ms以上。从而保证能够得到输出5V。

    所以启动时,启动输入电压至少为5V。

    这样,输出5V电压就有了,内部逻辑电路的供电就可以来自输出5V而不是来自于输入电压。

    所以,输入电压就可以最小工作在1.5V。(即使内部逻辑无法工作在1.5V,但是由于此时输出5V已经稳定了,内部逻辑电路可以从5V处得到供电。)

    谢谢。