Other Parts Discussed in Thread: TPS54316, TPS54312, TPS54314, TPS54314EVM
原理图参考芯片资料设计;频率设置为550KHz(即FSEL=5V,RT悬空);在使用这三个器件发现空载时,输出都只有0.89V左右;此时输入电压5V,三个器件每一个芯片电流竟然有0.05A。
给TPS54316加负载(约2K)输出只有1.5V左右;后来将TPS54316频率设置为700KHz,空载时约0.85V,加负载(约2K),输出为2.5V左右且不稳定;无法正常工作。
给TPS54312加负载(约70Ω)输出1.23V左右,正常工作。
给TPS54314加负载(约50Ω)输出0.5V左右,无法正常工作。
疑问,这个系列的芯片,空载0.89V输出是否正常?
如何解决TPS54316无法输出3.3V?