Other Parts Discussed in Thread: REF3133
您好 请问一下 REF3133AIDBZT这个芯片的推荐电路,谢谢
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
这个芯片外围没什么复杂的电路啊,你可以看下Datasheet第7页Figure2,另外第8页和第9页也有些典型应用。楼主可以描述一下你希望实现的功能。
我是想通过5V电压转出一个3.3V的精确电压,3.3V的电压通过精密电阻分压,得到0.12V的一个精确电压,0.12V的电压作为运放的输入,加到1个120欧姆的精密电阻上得到一个恒定的电流源,运算放大器外部5V电压供电,希望的要求是高精度,低噪声,纹波小,我想通过LM4128CMF-3.3,这个芯片是LDO还是基准源芯片,用这种芯片有没有要注意的地方
Hi
LM4128CMF-3.3这个芯片是高精度电压源, 这个芯片功能上和REF3133是一样的,产生3.3V基准。
你好 这个LM4128CMF-3.3 您能不能给一个推荐电路,那个恒流源的电路中,3.3V经过1K和33K的电阻分压,得到一个电压,加在120欧姆的精密电阻上,产生一个恒流源!恒流源应该是0.808mA