Other Parts Discussed in Thread: REF3133, LM4128
你好 我想得到3.3V的精确电压,用这个REF3133AIDBZT芯片可以吗?要求低噪声!请问一下 用基准源芯片和LDO的区别是什么
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
基准源和LDO的区别:基准源的初始精度和温飘等参数LDO好,但是输出电流一般比较小,请问下你是给什么东西供电?输出电流和噪声特性具体是多少?
Hi
REF3133是参考电压的芯片,所以你的要求不高是可以用这款芯片的,它的精度是0.2%.
如果你希望进度更加高可以用LM4128: http://www.ti.com.cn/cn/lit/ds/symlink/lm4128.pdf 精度是0.1%
或者是LM413:,http://www.ti.com.cn/cn/lit/ds/symlink/lm4132.pdf 精度0.05%.
Hi
基准芯片一般都是输出电流非常小,大部分在10mA左右,温飘非常小,精度非常高例如0.05%或者0.1%, 并且非常低的输出noise.
LDO是用于供电的,电流一般比较大,会是几十毫安到几安培,输出精度一般是2%左右,noise纹波也都比较低。
我是得到3.3V电压,是想通过分压得到一个稳定的0.12V,0.12V电压加在120欧姆的精密电阻上得到1mA的恒流源
Hi
能不能把你的电路提供出来看看,我觉得你这个方法产生恒流源是呼有问题,需要知道具体的电路才能再确认?