This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS63700测试电源静态电流以及效率疑问

最近测试老板公司的一块伽马能谱仪板上电源部分,电路中用到TPS63700,我在测试其静态电流的时候,得到的电流在4.2~5.2mA之间变动,测试的时候是不带负载,输入电压采用电源箱,参数为3.7V  500mA限流,电源箱电源正极输入部分串接电流表,电源-12V部分电路图如下(-12_EN已经拉高,输出端不接负载):

参考TI TPS63700的数据手册

虽然官方给的参数是-5V输出的电路测试的,-12V的静态电流也不应该达到4.2~5.2mA,电路以及PCB设计没有问题,用的是成熟可靠的设计,公司产品测试过,已经批量,我是调试几块作为学习。不知道Iq为什么这么大。请教论坛前辈,是不是我测试方法不对,还是焊接问题,还是静态电流就有这么大,数据手册中没明确给出-12V输出电路对应的静态测试电流。谢谢!!!

另外负载260Ω情况下,测得输入电路200mA,输入电压3.7V,负载电流48mA,负载电压-12.50V,效率能达到80%以上,跟数据手册能吻合。