This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ76940: 使用I2C读取单体电压时,存在部分失败

Part Number: BQ76940

在使用I2C进行单体电压读取时,部分单体电压(cell1~6)读取时,存在读取到异常值(0V,或者其他和实际电压不吻合的值)的情况(有的时候也能正常读取)。而相同的代码函数和时序可以正常读取其余剩余单体(cell7~15)的电压值

我现在的操作方法是直接单个字节依次读取各个对应寄存器内容,然后进行计算对应的单体电压

想请问一下,使用i2c读取单体电压时,是否存在什么特定的时序,注意的点,或者需要什么额外的操作?