TLV61220中未列明在实际使用时,如果配置的VOUT输出电压为2.3V 而Vin端口的电压为3.0V,这是如果将EN置为高,则会出现什么状况。
在实际应用中,由于由TLV61220从3.0V电池中取电并转换为所需的电压,当电池电压高于2.3V(单片机工作所需的最低电压),采用bypass方式,当低于2.3时才会采用boost模式,但是由于单片机并不知道电池的电压,当然可以通过AD转换得到,但AD转换也需要参考电压,但单片机也是从TLV61220获得电源,所以AD也没有办法,只有当电池电压低于2.3V时,才有可能从AD转换获得电池的电压,显然这一点是无法预知的,所以在本系统中,有必要将TLV61220始终配置在boost状态。