This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

UCC28780: 我想基于TIDA-01622方案UCC28780电源芯片进行修改,能否设计出DC180V1A的功率输出

Part Number: UCC28780
Other Parts Discussed in Thread: UCC27712, UCC24612

我想用UCC28780设计输出DC180V1A的输出,没有严格的电压文波电流文波高要求,但希望可以持续输出这个功率,在条件:瞬间负载时也就是2.6ms驱动负债,每秒驱动12次;这个条件下输出的平均功率大概再60W,压降不要低于160VDC即可满足要求。如果用UCC28780能否设计出?

能否不使用氮化镓开关管的情况下,使用NMOS与UCC27712半桥驱动器设计一个100KHz或200KHz的经典反激,想使用有源钳位回收尖峰损耗这个技术降低损耗提升一点效率。或者是否有合适的氮化镓开关管推荐。

数据手册推荐的配合UCC24612能否使用?

目前看到的有TI的TIDA-01622参考方案,想基于这个方案修改输出DC180V1A,有没有合适的下侧MOS开关管推荐,方案中使用的NV6115的Id耐流8A感觉不够,换成NV6117耐流12A不知道是否可以