工程师你好,
我们计划使用TPS61023,使4.5-4.7v输入变为5v 2a输出。
1.在TPS61023的规格书中,通过公式5,计算得知电感电流最小应选择2.8a的,是否证明可以选择温升电流等于3a的电感?
2.另外,规格书中,提到“The TPS61023 is designed to work with inductor values between 0.37 μH and 2.9 μH”,请问该感值是如何计算的?
3.若使用大于2.9uH的电感,会有什么风险呢?
感谢。
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
工程师你好,
我们计划使用TPS61023,使4.5-4.7v输入变为5v 2a输出。
1.在TPS61023的规格书中,通过公式5,计算得知电感电流最小应选择2.8a的,是否证明可以选择温升电流等于3a的电感?
2.另外,规格书中,提到“The TPS61023 is designed to work with inductor values between 0.37 μH and 2.9 μH”,请问该感值是如何计算的?
3.若使用大于2.9uH的电感,会有什么风险呢?
感谢。
Hi
可以的,甚至可以适当再大一些,防止更小的输入电压导致电感饱和。
按照你的参数计算即可,不一定必须是要在0.37uH~2.9uF, 即便超出不会有风险. 不过仍推荐在这个范围内,计算按照datasheet第13页,其中电感纹波电流为IL(DC)的30%.