Part Number: UCC28070
您好,
我的客户正在设计UCC28070电源,条件如下:
输入48VDC,输出96VDC,满功率1500W。目前存在的问题:目前调试功率在0-200w,会随着负载的加重直流输出电压会缓慢增加。100w负载时输出96.6v,200w时输出上升到99.16v。请问有办法让输出电压稳定在设定值吗?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
你的输入电容多大? 有没有用示波器测试输入电压,和输出电压是否稳定(还是说输出电压的变化是因为不稳定造成的)?
你好,输入侧没有电容,输入采用直流电源供电,是稳定的48V电压,在启动、带载、切载过程中均很稳定,用示波器测量。输出电压也很稳定,用示波器测量也几乎没有什么纹波。
HI
有没有确认芯片? 确认下Vsense脚是否损坏?
用示波器观测Vsense引脚,空载时输出电压稳定在目标电压时Vsense引脚为3.0V,但随着负载的加重,Vsense引脚电压会上升,200w负载时Vsnse引脚电压已上升到3.2V,请问这是否表示Vsense引脚损坏?
Hi
有没有确认Vsense的波形?将Vsense的电容加到到3.3nF, 另外再确认一下电压补偿电路。