您好,学习成功了,充电的时候,为什么还没有充满就显示充满了呢?FC置位了,在学习期间也有这样的问题。我的设置Taper current=350mA,cell taper Voltage=170mV,current Taper Window=40seconds;充电电流还有500多mA的时候就显示充满了,充电截止电流都没有到350mA以下,判断充满的条件不是不满足吗?怎么就判断充满了呢?希望能帮忙看下3531.6_13.gg.csv3240.test6-13.log
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
您好,学习成功了,充电的时候,为什么还没有充满就显示充满了呢?FC置位了,在学习期间也有这样的问题。我的设置Taper current=350mA,cell taper Voltage=170mV,current Taper Window=40seconds;充电电流还有500多mA的时候就显示充满了,充电截止电流都没有到350mA以下,判断充满的条件不是不满足吗?怎么就判断充满了呢?希望能帮忙看下3531.6_13.gg.csv3240.test6-13.log
搜索
复制
您好,需要同时满足下面三个条件。Current Taper method:
a. During two consecutive periods of Current Taper Window, the AverageCurrent() is less than Taper Current AND
b. During the same periods, the accumulated change in capacity > 0.25 mAh /Taper Current Window AND
c. Voltage() is > Charging Voltage – Charging Taper Voltage. When this occurs, the [CHG] bit of Flags() is cleared. Also, if the [RMFCC] bit of Pack Configuration is set, and RemainingCapacity() is set equal to FullChargeCapacity().