This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS65133: 输出正负电压没有达到±5V

Part Number: TPS65133

使用TPS65133希望获得±5的电压,按照官方的原理图画的板子,但是在测试的时候发现其VPOS的平均电压为4.842V,VNEG的平均电压为-5.208V。测试过程中没有接负载,直接接到了示波器上。

但是我希望获得±5V的电压,其值稳定在±4.9V~±5.1V之间。我应该怎么做?

下面是我的电路图和PCB布局: