Other Parts Discussed in Thread: TPS61230, LM3478, LM3488
这个Switch Current Limit 跟 输出电流大小是怎么个对应关系?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi
在升压架构中Switch Current Limit 电流与输入电流关系比较大,但是可以从输出电压折算过来:
例如输入是 Vin/Iin, 输出是Vo/Io, 效率是n 频率是f
那么输入电流就是Vo*Io/(n*Vin), 电感的纹波电流是 Vin(Vo-Vin)/ (L*f*Vo)
而最小的电流限制Switch Current Limit 需要大于输入电流Iin + 纹波电流/2
所以是IswL > Vo*Io/(n*Vin) + Vin(Vo-Vin)/ (2L*f*Vo)
我现在需要找一款 升压芯片 用于电池电压较低时升压用, 输入在3.0—3.8V左右 输出4V 输出电流3A 后面接了11W左右负载 。TI这边我看了几款IC TPS61230 和TPS61280 。就是不知道怎么看是否满足输出电流要求
你好,基本是对的,驱动电流峰值1A,1A的驱动电流大概可以做到10A的功率,也不是无限大的,谢谢。