Other Parts Discussed in Thread: TPS61200, TPS61201, TPS63050
Hi Ti,
Our application is 3 AAA battery (0.9V~1.7V) connect to TPS62743 VIN.
If the VOUT of TPS62743 is set as 3.3V, but when battery become empty, the VIN is lower than the VOUT .
Does it will cut off the output? or just output the voltage which is same as VIN?
Thank you!
Best Regards,
Scott