This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25720: 充电过程中停止充电,BQ25720无输出

Part Number: BQ25720


适配器15V 2A,最小输入电压11.2V,充电电流1.35A,4s电池16.8V。

充电过程中概率性停止充电,停止充电瞬间读取寄存器值如下,可以看到进入VINDPM模式,输入电压回读为11.1V。

请问:

1、BQ25720是什么原因导致无输出(此时系统电压是电池提供,断开电池整机断电,判断BQ25720无输出)?

2、有什么办法可以避免触发该事件